AXIS#.GEAR.AUTOSTART

Description

The command AXIS#.GEAR.AUTOSTART determines whether or not gearing begins when the axis is enabled or transitions into Command Source: Electronic Gearing.

If AUTOSTART is enabled then electronic gearing immediately begins and tries to achieve synchronization with the master.

If AUTOSTART is disabled, issue AXIS#.GEAR.MOVE before synchronization begins.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type

Parameter

Description

Determines whether gearing autostarts or requires manual start.

Units

N/A

Range

0 (Disabled) – 1 (Enabled)

Default Value

1 (Enabled)

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Fieldbus Information

CANopen Over EtherCAT (COE)

Name

Index

SubIndex

Access

PDO Mappable

AXIS1.GEAR.AUTOSTART

5006h

5h

Read/Write

No

AXIS2.GEAR.AUTOSTART

5106h

5h

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

AXIS#.GEAR.AUTOSTART

5507

1583

Unsigned8
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
AXIS1.GEAR.AUTOSTART

5006h

05h

Unsigned8

-

-

Read/Write

No

AXIS2.GEAR.AUTOSTART

5106h

05h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.GEAR.AUTOSTART

5507

1583

Unsigned8

Read/Write

-

AXIS2.GEAR.AUTOSTART

71043

1158

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.GEAR.AUTOSTART

5507

Unsigned8

Read/Write

-

Related Topics

Electronic Gearing